Establishing the safety and security of medical device software is critical to protect patients. The IEC 62304 standard provides a…
If testing and protecting your device from known issues, is equivalent to closing a treasure vault’s door, by that analogy,…
More than ever, embedded devices of today are leaning on open source solutions like Linux. The ease, versatility, and flexibility…
Nowadays, most embedded systems are built using 32-bit CPUs. These devices give plenty of scope for performing the arithmetical processing…
I recently wrote a blog post about a number puzzle, which provoked a few interesting comments. One of them, in…
Just about all the embedded CPU manufacturers produce evaluation boards employing their devices with a suitable selection of peripherals.These boards…
I quite like puzzles and “brain teasers”. Although I would never describe myself as a mathematician, I do like playing…
As I talked about last week, the news lately has been dominated by the Olympics, but NASA managed to grab…
If you had asked me about the Olympics two weeks ago, I would have dismissed the discussion with “I don’t…
Most of the time, I subscribe to the view that “the only stupid question is the one you did not…
I recently wrote about the concept of having fun. At the time, I commented that happiness is easier to identify,…
From time to time I am pleased to receive submissions from colleagues, who can give different perspectives on embedded software….