Products

Finally – digital Standards are available ! And you are able to use them with Polarion !

When I started using Polarion as a Quality Manager back in 2014, I directly fell in love with the possibility to granularly link single requirements to single risks, single tasks, single testcases etc etc. The only thing I missed then was to also link a product requirement with a requirement in a standard, like ISO 13845, DIN EN 13637 etc – which only were available as PDFs or printed versions then. So I did a lot of different experiments to somehow granularly address one requirement inside this standard from Polarion, and ended up in some ugly Copy’n-Paste-action. ☹

I dreamed :“How cool would it be if I could import these standards in a smarter format, maybe even pre-attributed by  the authors, so that I can have those single requirements as single, linkable, categorized workitems in Polarion ? Sigh…”

Now the time has come. And we will demonstrate it to you in a webinar on 2024-06-04 . You can register here : www.polarion.com/normen
P.S: We will have more follow-up webinars about this topic in future. This first one will be in german language.

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.stage.sw.siemens.com/polarion/finally-digital-standards-are-available-and-you-are-able-to-use-them-with-polarion/