Never trust a TLA (three-letter acronym) or those who use them, unless the abbreviation provides some value in terms of…
Wiki quote: “A grille is an opening of several slits side by side in a wall or metal sheet or…
Considering that CFD (Computational Fluid Dynamics) is an advanced mathematical method for predicting fluid flow and heat transfer using a computational…
Larry Grayson’s famous high camp catchphrase would be well heeded by those wanting to ensure good thermal insulation. You can make…
The Mentor ‘IDEAS for Mechanical’ site allows users of FloTHERM, FloVENT, FloTHERM PCB and FloEFD to post their software enhancement requests (access…
Conduction, the transfer of heat through a solid object. Convection, the transfer of heat in moving air/fluid. Radiation, the transfer…
Electronics cooling involves ensuring that IC package temperatures do not exceed maximum rated values. If they do the probability of thermo-mechanical…
Why is it that when you increase a cavity air gap size beyond ~30mm is there no subsequent detrimental affect…
100mm block, 50mm insulation, 50mm cavity air gap then 100mm block make up an external wall that in theory comply…