Products

How to measure ISO 26262 metrics of analog circuitry

By Stephen Sunter  – Mentor, A Siemens Business

ICs designed for safety-related automotive systems are expected to operate safely for the lifetime of the vehicle. The manufacturing test strategy and on-chip runtime test capabilities are important aspects of achieving that zero-DPPM goal.

Much discussion of test and diagnosis for automotive ICs addresses digital logic and memories, but most (70% or more) of the field failures occur in the mixed-signal portion of the chip. These defects, even in small numbers, can’t be tolerated in safety-critical automotive applications. Mentor developed the Tessent DefectSim analog defect simulator to address this growing need for analog test tools. Tessent DefectSim automates the job of measuring a circuit’s tolerance to defects.

 

The ISO 26262 standard provides for defect tolerance. Since the focus of the standard is minimizing the likelihood of unsafe failures, the likelihood of each fault/defect must be estimated to be able to compute these metrics. The metrics include:

 

  • Single point fault metric (SPFM)
  • Probabilistic metric for random hardware failures (PMHF)
  • Residual faults (DC-Residual)
  • Latent faults (DC-Latent)
  • Latent fault metric (LFM)

 

All but LFM can be measured by Tessent DefectSim by injecting on defect at a time. LFM cannot be measured by injecting one defect at a time since, by definition, latent defects do not individually cause any failure. With Tessent DefectSim, a two-step procedure is used to overcome this limitation when measuring LFM. Figure 1 shows a simplified Venn diagram of the different outcomes of simulated injected defects.

 

Tessent DefectSim automatically measures all these metrics. It can also simulate entirely digital circuits but inject transistor-level defects instead of gate-level stuck-at faults. This allows IC designers to provide an automated and objective assessment of likelihood-weighted defect coverage and defect tolerance, in less time, when these metrics are required by Tier 1 automotive customers.

 

For details on how Tessent DefectSim measures the fault metrics for analog circuits, download the whitepaper Measuring ISO 26262 Metrics of Analog Circuitry in ICs.

Leave a Reply

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.stage.sw.siemens.com/tessent/2018/04/17/how-to-measure-iso-26262-metrics-of-analog-circuitry/